Configure a range transitioned event
    Trigger methods if the value of a variable or object property is in or out of a specific range.
- InProject view, select an object or a variable.
- InProperties, right-click a variable or a property and select .TIP: If needed, selectto add a variable. 
- InEvents, fromTransitionselect:- In (Exclusive) 
- Out (Exclusive) 
- In (Inclusive) 
- Out (Inclusive) 
 ItemDescription Range Range Value transition Value transition Method execution Method execution
- Set theFromproperty.TIP: You can enter the threshold value or add a dynamic link to the threshold value. For more information about dynamic links, see Create dynamic links.
- Set theToproperty.TIP: You can enter the threshold value or add a dynamic link to the threshold value. For more information about dynamic links, see Create dynamic links.
- Next toVariableTransitioned, select. 
- Select a method:- For global methods, expandCommands.
- For local methods, expand the nodes that expose methods (for example, aDataGridnode exposes aRefreshmethod), or expand the node related to a specific NetLogic.
 
- (optional) If the method requires arguments, expand the method and set arguments.
- (optional) Select additional methods.
out of range
range event
    
Provide Feedback