Use cases
    Filter data using an SQL query to display specific data from the database.
You can compose a query:
      
- As text
     TIP: 
    Do not specify the table name in the 
FROM
 clause. Specify the table name in the dynamic link to the BrowseName
 of the table with an {0:sql_identifier}
 placeholder in a string formatter.Use case: filter by time
      Use the 
Time
 or Timestamp
 column that contains the date and time to filter data by time.Use the 
sql_literal
 literal in the placeholder of the string formatter. Consider using a temporary DateTime
 variable.Example. Export records that have a Timestamp greater than a certain instant of time:
        
SELECT * FROM {0:sql_identifier} WHERE Timestamp > {1:sql_literal}
Example. Export records that have a Timestamp between two instants of time:
        
SELECT * FROM {0:sql_identifier} WHERE Timestamp BETWEEN {1:sql_literal} AND {2:sql_literal}
Use the Timestamp column to create a time filter on a Logger. Use the Time column to filter alarm history.
Use case: filter by alarm severity
      The 
Severity
 column contains the value of the severity of an alarm. Use this column to filter various severities of an alarm grid or alarm history grid.Example. Export the history of alarms with severity 1:
        
SELECT * FROM {0:sql_identifier} WHERE Severity = 1
Example. Export the history of alarms with severity between 1 and 3:
        
SELECT * FROM {0:sql_identifier} WHERE Severity BETWEEN 1 AND 3
Use case: filter by alarm or variable
      The 
ConditionName
 column contains the name of the alarm. Filter archived alarms to obtain specific alarms. You can filter alarm names if they follow a specific pattern.The condition can be used on the 
SourceName
 column to filter by the input variable.Example. Export the alarm history with a given BrowseName in the past:
        
SELECT * FROM {0:sql_identifier} WHERE ConditionName = {1:sql_literal}
Example. Export the history of the alarms connected to the variable:
        
SELECT * FROM {0:sql_identifier} WHERE SourceName = {1:sql_literal}
Example. Export the history of alarms starting with Exclusive:
        
SELECT * FROM {0:sql_identifier} WHERE ConditionName LIKE 'Exclusive%'
Use case: filtering Recorded Alarms
      Export some columns of the logger.
Example. Export the alarm history with only the Italian columns:
        
SELECT "ActiveState_it-IT", "AckedState_it-IT", "ConfirmedState_it-IT", "ConditionName", "EnabledState_it-IT", "SourceName", "Time", "Message_it-IT", "Severity" FROM {0:sql_identifier}
Provide Feedback