Create an ODBC database
    Create a database object that fetches data from an SQL server or a MySQL server.
Prerequisites
To connect to an ODBC database from 
Windows®
 devices: - Install one of these ODBC drivers:- MySQL Unicode
- ODBC Driver 17 for SQL Server
 
- Configure the ODBC data source. See Administer ODBC data sources - Microsoft Support.
- InProject view, right-clickDataStoresand selectODBC database.
- InProperties, inDBMS type, select the type of the database server.
- InProperties, complete:- Configuration:- DBMS type. EitherSQL ServerorMySQL.
- (optional)DSN(Data Source Name). Applicable only forWindowsdevices.IMPORTANT:If specified, the DSN automatically provides the ODBC connection properties.You cannot overwrite the DSN properties by manually completing theServer,TCP Port,Database,Username, andPasswordfields.
- Server. IP address or hostname of the database server.
- TCP Port. TCP port of the database server.TIP: The default 0 value resolves to 1433 for SQL servers and 3306 for MySQL servers.
- Database. Database name in the database server.TIP: Providing the database name is optional if the database name is specified in the ODBC connector.
- Username. Name of the user that can access the database.
- Password. Password of the user that can access the database.
 
- Store and Forward:TIP: Store and Forward stores data in case of temporary connection loss to storage. See Store and Forward.- SF Enabled. Enables or disables Store and Forward.
- SF Buffer Max Size. Maximum number of elements in the buffer, which can be set from 1 to 100000. An element is one entry (row) in a database table.
- SF Buffer Overwrite. When set toTrue, overwrites oldest entries with new data when the buffer limit is reached. When set toFalse, ignores new data when the buffer limit is reached.TIP: The following diagnostic, read-only properties are available:SF Buffer usage. Displays the current number of elements in the buffer.SF Buffer overflow. False - indicates that currently upcoming data is handled. True - indicates that the buffer is full and currently upcoming data is ignored.
 
 
(optional) Configure the database structure. See Configure a database table.
Provide Feedback