Create a remote Influx database
    
     TIP: 
    Remote Influx database does not support InfluxDB cloud.
- InProject view, right-clickDataStoresand selectRemote InfluxDB database.
- InProperties, complete:- Properties:- Server. IP address or hostname of the database server.
- TCP Port. TCP port of the database server.TIP: The default value for InfluxDB servers is typically 8086.
- Organization. Organization must match the one specified on the database server.
- Bucket. Bucket must match the one specified on the database server.
- Token. Token must match the one specified for fetching data from the database server.
- Use SSL. For secure data connection, set toTrue.
- Server Certificate. Server certificate must match the one specified on the database server for secure SSL connection.
 
- Store and Forward:TIP: Store and Forward stores data in case of temporary connection loss to storage.Store and Forward is only available for external Influx databases. See Store and Forward.- SF Enabled. Enables or disables Store and Forward.
- SF Buffer Max Size. Maximum number of elements in the buffer, which can be set from 1 to 100000. An element is one entry (row) in a database table.
- SF Buffer Overwrite. When set toTrue, overwrites oldest entries with new data when the buffer limit is reached. When set toFalse, ignores new data when the buffer limit is reached.TIP: The following diagnostic, read-only properties are available:SF Buffer usage. Displays the current number of elements in the buffer.SF Buffer overflow. False - indicates that currently upcoming data is handled. True - indicates that the buffer is full and currently upcoming data is ignored.
 
 TIP:InfluxDB datastore has additionalTagsproperty for each table created to assign InfluxDB tags to dataset. InfluxDB tags are used by Influx database to identify and label datapoints for further analysis. It is also the way to log datapoints with the same timestamp to the same bucket and measurement, and avoid loss of data.For example: Without tags defined, when many events are triggered at the same time (with the same timestamp), InfluxDB overwrites them and only one record is logged in the database. To avoid this, you can bind theTagsproperty to a unique property of a logged event (such asAlarm Name). This forces the InfluxDB server to record all datapoints with the same timestamp. You may use theTagsproperty to add any variable as a label for datapoints, for maintaining and analyzing data stored on server.
(optional) Configure the database structure. See Configure a database table.
Provide Feedback