Configure a communication driver
    Configure a communication driver to import tags in the online or offline mode.
Prerequisites
- Learn about any specific considerations for your controller. See Communication drivers overview.
- If you import tags in the offline mode, export tags from a supported controller to a file. See the controller user assistance.
- To configure a communication driver
- From the toolbar, select.Open dashboard page
- SelectConfigure communications to devices.
- SelectNew station.
- Select a station type.
- (optional) Edit the name of the station.
- SelectNext.
- Fill in the properties and selectNext.
- SelectNext.
- Configure tags import for the station:TIP:Some communication drivers may not support importing tags from controllers in the online mode, offline mode, or both modes.To import tags, you must be logged on to the FactoryTalk Network.- To import tags in the online mode, set the toggle toOnline.
- To import tags in the offline mode, set the toggle toOfflineand inFile path, provide a path to the file with exported controller tags.
 TIP: To select the station object inProject view, selectSelect in property view.TIP: If you import FactoryTalk Design Studio tags offline, any routine scoped tags are imported and referenced in the FactoryTalk Optix Application. However, if you then deploy the FactoryTalk Design Studio project through Logix Designer, any routine scoped tags are not deployed or downloaded to the controller because Logix Designer does not support routine scoped tags. Therefore, if you deploy that FactoryTalk Optix Application to a runtime device and connect the application to the controller, the routine scoped tag references display an error at runtime because the tags were not downloaded to the controller.
- Select the tags of interest and selectNext.
- (optional) To configure another communication driver, selectConfigure another deviceand repeat the procedure.
- SelectExit.
In 
Project view
, the variables corresponding to the selected tags are added.If you imported tag types, create instances from the imported tag types. See Create an instance of a tag type.
communication
communication driver
    
Provide Feedback