TwinCAT driver
    Observe these guidelines when working with TwinCAT driver.
Supported controllers
      The driver supports these controller families:
        
- TwinCAT® runtime
- Beckhoff ® TwinCAT® systems
     IMPORTANT: 
    The driver has been tested with TwinCAT® runtime and CX5130-0155.
Controller tags import
      
     IMPORTANT: 
    
        Before importing tags from Beckhoff ® TwinCAT® controllers, perform Configure controller routing.
You can import tags in these modes:
        
- Online mode
- Use online mode to import tags directly from the controller at design time or runtime.
- Offline mode
- Use offline mode to import tags fromTPYfiles.For more information, refer to the product documentation.
  This communication driver supports importing custom data types defined in the
        controller project.
Data types
      The driver supports these data types:
        
  
    
| Controller data type | FactoryTalk Optixdata type | Length | Notes | 
|---|---|---|---|
| BOOL | BOOL | 1 BIT | |
| BYTE | BYTE | 1 BYTE | |
| WORD | UINT16 | 2 BYTES | |
| DWORD | UINT32 | 4 BYTES | |
| LWORD | UINT64 | 8 BYTES | |
| SINT | SBYTE | 1 BYTES | |
| INT | INT16 | 2 BYTES | |
| DINT | INT32 | 4 BYTES  | |
| USINT | BYTE | 1 BYTE | |
| UINT | UINT16 | 2 BYTES | |
| UDINT | UINT32 | 4 BYTES | |
| LINT | INT64 | 8 BYTES | |
| ULINT | UINT64 | 8 BYTES | |
| REAL | FLOAT | 4 BYTES | |
| LREAL | DOUBLE | 8 BYTES | |
| TIME | DURATION | 4 BYTES | |
| LTIME | DURATION | 8 BYTES | |
| DATE | DATE TIME | 2 BYTES | |
| TIME_OF_DAY(TOD) | UTC TIME  | 4 BYTES | Rockwell Automationrecommends using the Date and time object, which allows you to set and view date and time data. | 
| DATE_AND_TIME(DT) | DATE TIME | 4 BYTES | |
| STRING | STRING[Length]  | ||
| WSTRING | STRING[Length] | ||
| ARRAY 1 dimensional | Type [dimension] | ||
| ARRAY 2 dimensional | Type [1st dimension, 2nd dimension] | ||
| ARRAY 3 dimensional | Type [1st dimension ,2nd dimension, 3rd dimension] | 
twincat
twincat driver
    
Provide Feedback