Configure the authentication mode
    Change the default authentication mode to allow local users and domain users to log on at runtime.
Prerequisites
To allow Active Directory users to authenticate, either:
        
- Obtain the Active Directory domain name and server address.
- Ensure that theWindowsclient is joined to the Active Directory domain.
To allow LDAP users to authenticate, obtain:
        
    
    
- LDAP server address
- Base64 CA certificate file exported from the Active Directory server or from a computer in the domain
     TIP: 
    
FactoryTalk Optix Studio
 does not support LDAP over SSL (LDAPS).- To configure the authentication mode
- InProject view, select the root node.
- InProperties, expandAuthentication, and then inAuthentication mode, select an authentication type:- Model only. Users created inFactoryTalk Optix Studio.
- Local only. Local machine users.
- Domain only. Active Directory and LDAP users.
- Domain and local. Active Directory, LDAP, and local machine users.
- Domain, local, and model. Active Directory and LDAP users, local machine users, and users created inFactoryTalk Optix Studio.
- OAuth 2.0. Users authorized with the OAuth 2.0 protocol.
 
- Configure properties for the selected authentication mode.For more information, see Authentication properties.
authenticate
authentication
    
Provide Feedback