Create a dynamic link using an alias
    Create a dynamic link to use an existing alias as a shortcut. Dynamic links help prevent having to look up the same source node repeatedly.
- InProject view, select a node that has the property value that you want to set through the dynamic link.
- InProperties, in the property of interest, select. Add Dynamic Link Add Dynamic Link
- Expand either theAliasesfolder or thePanel loadersfolder to select the alias nodeto display. The information model to which the alias points and the source node of the dynamic link appear.TIP: In thedynamic linkswindow, the aliases that you create appear in theAliasfolder. Aliases in theDynamic panelfolder are generated automatically. The information model to which the alias points and the source node of the dynamic link appear.TIP: In thedynamic linkswindow, the aliases that you create appear in theAliasfolder. Aliases in theDynamic panelfolder are generated automatically.
- Select the source node of interest and then chooseSelect.
The path to the reference node or attribute appears in the property.
dynamic link
    
Provide Feedback