Shelve and unshelve alarms
    Shelve and unshelve alarms at runtime. Shelving alarms prevents the notification of new
    state changes. Shelve duration is assigned to the alarm in the project.
- At runtime, in theAlarm manager, select the alarm to modify.
- Perform one of the following actions:- To timed shelve the alarm, selectTimed-Shelve, select the shelve duration, and selectShelve.
- To one-shot Shelve the alarm, selectOne-Shot Shelve.
- To unshelve the alarm, selectUnshelve.
 
shelve
unshelve
    
Provide Feedback