Alarm summary
    Use the 
Alarm summary
 widget to display essential information about all retained, and not currently shelved, alarms in a project.Overview
      Use the 
Alarm Summary
 to:
        - acknowledge alarms
- disable alarms
- shelve alarms
- sort alarms
- filter alarms
- view alarm details
- reset latched alarms
- confirm alarms
- suppress alarms
- see a rollup of alarm counts
The 
Alarm summary
 widget displays the following columns of information:| Column | Description | 
|---|---|
| Priority | Alarm priority. The following values are available:
                 
 | 
| Status | Alarm status. The following values are available:
                 
 | 
| Event time | The time the alarm condition or sub-condition changed to the currently displayed state. | 
| Condition name | Displays alarm condition. The Condition name field display value depending on the alarm logic | 
| Confirmed | Specifies if the alarm is confirmed or unconfirmed | 
| Name | Name of the alarm object that generated the alarm event.  | 
| Message | Message associated with the alarm event. For example, if HH is active, message dedicated for HH displays. In alarm details popup, message with higher priority displays. | 
| Source variable | The variable monitored by the event. | 
In 
Properties
, you can select which alarm summary table columns display, and disable or hide specific buttons.Provide Feedback