View alarm log events in UTC time zone
    At runtime, the 
Data Grid
 object of the Alarm History Grid
 widget displays the date and time in the Timestamp
 column. The time appears in the local time zone of the device using the LocalTime
 property of the events. View alarm log events in the UTC standard time zone by configuring the Time
 property of events.- In the main toolbar, select.Template Libraries
- InTemplate Libraries, fromWidgets, drag theAlarm History Gridobject to the desired folder in theUIfolder.The widget appears in the node.
- With theData gridof the widget selected, in theTextproperty of theTimestampor other column, select. Change Dynamic Link Change Dynamic Link
- In the Dynamic Links window, select .
- ChooseSelect.
Provide Feedback