Create an Alarm grid
    Create an 
Alarm grid
 to display the status of each alarm in a row.- Customize the objects included in theAlarm gridto change the appearance of the grid and display specific alarm information.
- In the main toolbar, select.Template Libraries
- InTemplate Libraries, selectWidgets.
- UnderComponents, dragAlarm Gridto a folder in theUIfolder.AlarmGrid# (type)appears.
- InTemplate Libraries, selectClose.
- (optional) On the editor, select the alarm grid and the buttons of the alarm grid to customize thePropertiesandEventsof the grid and buttons. For example, to change the appearance of the grid:- Row color. Select the background color row or selectto bind to a tag with the value of the color. Add Dynamic Link Add Dynamic Link
- Row text color, Select the color of the text in the alarm grid or selectto bind to a tag with the value of the color. Add Dynamic Link Add Dynamic Link
 
- (optional) To display additional alarm information at runtime, select theAlarmsDataGridand add columns:- InProperties, afterColumns, selectand select the type of column to appear at the right end of the grid: - Text column. A column with static text.
- Editable text column. A column with text that you can edit at runtime.
- Image column. A column that displays a graphic.
 
- InProperties, expandColumnsand scroll to the new columnDataGridColumn#.
- InTextfor the column, select. Add Dynamic Link Add Dynamic Link
- In the Dynamic Link window, navigate to , and then select the property for the alarm event.To view properties by alarm type, expand alarm events, identified by. TIP: By default, theAlarm griddisplays all of the enabled and active alarms. To display only certain alarms at runtime, see Create an alarm filter. TIP: By default, theAlarm griddisplays all of the enabled and active alarms. To display only certain alarms at runtime, see Create an alarm filter.
 
alarm condition
alarm grid
row color
text color
    
Provide Feedback