View alarms in remote local time zone
View alarms in the local time zone to view alarm events remotely.
- Select.Template Libraries
- InTemplate Libraries, drag theAlarm gridorAlarm history gridobject fromWidgetsinto a node in theUIfolder.
- In
- InProject view, select the alarm object.
- InProperties, expandTimestamp.
- InText, reset the current value and then select.
Change Dynamic Link - At the bottom of the window, selectAdvanced...
- In the Advanced Dynamic Link editor, select
Insertand then selectExpression evaluator. - InExpression, type{0} + {1}and then pressEnter.
- In the{0} DynamicLinkpane, selectand then select .
Change Dynamic Link - In{1} DynamicLink, selectand then select .
Change Dynamic Link - ChooseSelect.
Provide Feedback