Import nodes at runtime
Importing nodes at runtime requires an initial configuration.
Prerequisites
- To import nodes at runtime
- InProject view, select an OPC UA client.
- InProperties, selectnext to
Runtime configurations.RuntimeConfigurationappears under#Runtime configurations. - Set theRuntimeConfigurationproperties:#
- Local destination node. Design node where the node of interest and all its children are imported.
- Remote source node. Path of the node of interest in the server information model starting, expressed as the sequence ofseparated byBrowseName/. Selects all child nodes of the indicated node. You do not need to indicate the server root node.
- Content synchronization mode:
- No synchronization. Disable the import of nodes and variable values.
- Import only. Import the nodes of interest but do not retain the node structure or the values of synchronized variables.
- Import and synchronize values. Import the nodes of interest and keeps the variable values synchronized.
- Full synchronization. Import the nodes of interest and keep their structure and the values of the variable synchronized.
- Include remote source node:
- False. Imports child nodes only.
- True. Imports both the node indicated in the remote source node and the child nodes.
- Enable event synchronization. In the OPC UA client node indicated inLocal Destination Node, shows the events generated by the server node indicated in Remote Source Node.
- Event type. Event type of interest among those generated by the server node indicated in Remote Source Node and shown in the OPC UA client node indicated inLocal Destination Node.TIP: Selectand inside , select the event type.
Add Dynamic Link
Provide Feedback