Draw a polyline or polygon
Use the
Polyline
tool to draw a polyline or polygon.- FromProject view, open the window to contain the object.
- In the editor toolbar, select
Polyline. - In the window, position the crosshair where the polyline or polygon is to begin.
- Draw the shape:
- Polyline. Select points on the screen. Pressto finish drawing the shape.Esc
- Polygon. Select points on the screen and then select the initial point to close the polygon. If you do not want the last line segment to connect with the first line segment, holdwhen positioning the last line segment.CtrlTIP: To change the shape of a polyline or polygon, select and drag the sizing handle of a segment.
The object appears in the window and in
Project view
.Provide Feedback