Rename a graphic object
Rename a graphic object to give it a unique name. Rename a graphic object after adding an instance of or copying the object.
- In the window orProject view, select the graphic object.
- InProperties, inName, select the name or selectand then type the new name of the graphic object.

Provide Feedback