Linear gauge
    Set and/or display a whole number value within a range of possible values.
Properties
			
  | Name | BrowseName | DataType | Description | 
|---|---|---|---|
| Value change behavior | ValueChangeBehaviour | Mode of updating text when the user writes in the text box. At end of typing = update the value after the user has pressed Enter with either physical or virtual keyboard (pressing Esc or clicking outside the object, the previous text is restored); When typing = in real-time when writing. | |
| Colorization mode | ColorizationMode | Set the colorization mode which will be used when applying the selected color to the image. | |
Events
			Modified value
- BrowseName
Provide Feedback