Objects and types
An object is an element that represents a physical or non-physical component in the project. A type is a model or template object for creating instances of an object.
Create objects from
Project view
or Type view
. Any graphic object that you create in the default UI
folder or a subfolder of the UI
folder is automatically configured as a type. Types are available in Type view
in the UI
folder.Change the properties of an object or type instance to change the appearance and data values displayed for that instance at runtime.
Provide Feedback