Alarm events
Each alarm type has a specific event in the
Properties
pane. There are three default methods for each alarm event:
- Acknowledge. Acknowledge the alarm.
- Add comment. Add a comment to the alarm in the alarm grid.
- Confirm. Resolve the cause of the alarm.
Alarm type | Alarm event |
---|---|
Digital alarm | OffNormalAlarmType |
Exclusive level alarm | ExclusiveLevelAlarmType |
Exclusive deviation alarm | ExclusiveDeviationAlarmType |
Exclusive rate of change alarm | ExclusiveRateOfChangeAlarmType |
Non-exclusive level alarm | NonExclusiveLevelAlarmType |
Non-exclusive deviation alarm | NonExclusiveDeviationAlarmType |
Non-exclusive rate of change alarm | NonExclusiveRateOfChangeAlarmType |
Provide Feedback