Range

Allows to describe the minimum and maximum value of a variable and to enable the value constraint.
BrowseName
RangeType
SuperType
PropertyType(PropertyType)

Properties

Name
BrowseName
DataType
Description
Low limit
Low
Low limit
High limit
High
High limit
Constrain
Constrain
Enables or disables the constraint on the variable value
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.