Ellipse

Ellipse that can be adapted according to the design needs.
BrowseName
Ellipse
SuperType
Container(Container)

Properties

Name
BrowseName
DataType
Description
Border color
BorderColor
Color of the polygon border.
Fill color
FillColor
Fill color of the polygon area.
Border thickness
BorderThickness
Border thickness in pixels.
Hit test visible
HitTestVisible
True = intercept user clicks. False = does not intercept user clicks, which are instead passed to the underlying object, based on the order on the Z axis.
Blink
Blink
Allows the object to periodically blink, ignored when the object is not visible.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Events

MouseDown event
BrowseName
MouseUp event
BrowseName
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.