OMRON Fins Tag

BrowseName
OmronFinsTag
SuperType
Tag(Tag)

Properties

Name
BrowseName
DataType
Description
Memory area
MemoryArea
Controller memory location in which to read/write the tags.
Data conversion
DataConversion
BCD format
BCDFormat
Maximum length
MaximumLength
(string data only) Maximum number of characters in the string.
Word address
NumWord
Address in the memory location in which to read/write the tags.
Bit number
BitOffset
Specify the position of the bit in the word.
Flag address
NumFlag
Bank number
BankNumber
Array update mode
ArrayUpdateMode
(Inherited from Tag)
Original data type
OriginalDataType
(Inherited from Tag)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.