Dynamic link
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Parent variable index | ParentArrayIndex | Limits the action of the dynamic connection to a single element of the parent variable if it is an array. The default value (-1) indicates that it has not been set. | |
Provide Feedback