- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
IUANode.GetNodesByType<T>()
Returns an
IEnumerable
C# list that corresponds to the list of child nodes of the node on which the method is invoked and of the specified type.
TIP:
In Visual Studio and Visual Studio Code, specifying the exact type (
<T>
) improves the intelligent code completion and makes it easier to identify errors while writing the code.At runtime, it is evident if the node searched is of the requested type. If the searched node is not of the requested type, the API returns
null
.IEnumerable<T> GetNodesByType<T>();
Arguments
- T
- AnIUANodeC# class that corresponds to the class of the C# object to return.
Returns
- IEnumerable
- A C# list that contains the nodes of the requested type.
Example
var model = Project.Current.Get("Model"); var motors = model.GetNodesByType<Motor>();
Provide Feedback