Configure the AlarmImporter NetLogic

Integrate the NetLogic with your project.
  1. In
    Project view
    , select
    AlarmImporter
    .
  2. In
    Properties
    , at the top, select
    Add new dd
    Variable
    .
  3. Hover-over the variable, select
    Edit
    , and enter
    CSVPath
    .
  4. Select
    Int32
    and select
    AbsoluteResourceUri
    .
    TIP: If you do not see the required option, select the
    Show all
    check box.
  5. Remove the variable value.
    The variable value is empty.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal