Create a motor values widget (type)

Create container elements for gauges, labels, and text boxes related with selected motor values.
  1. Crate the motor values widget panel:
    1. In
      Project view
      , right-click
      UI
      and select
      New
      Containers
      Panel
      .
    2. Hover-over the panel, select
      Edit
      , and enter
      MotorValuesWidget
      .
  2. Create an alias to the motor instances:
    1. In
      Properties
      , at the top, select
      Add
      and select
      Alias
      .
    2. Double-click
      Alias1
      and enter
      Motor
      .
    3. Create a dynamic link between
      Kind
      and
      ProjectName
      Model
      MotorType (type)
      For more information about dynamic links, see Create dynamic links.
  3. Crate a motor speed panel:
    1. In
      Project view
      , right-click
      MotorValuesPanelWidget
      and select
      New
      Containers
      Panel
      .
    2. Hover-over the panel, select
      Edit
      , and enter
      MotorSpeedPanel
      .
  4. Crate a motor acceleration panel:
    1. In
      Project view
      , right-click
      MotorValuesWidget
      and select
      New
      Containers
      Panel
      .
    2. Hover-over the panel, select
      Edit
      , and enter
      MotorAccelerationPanel
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.