Advanced features concepts
IMPORTANT:
FactoryTalk Optix Studio
supports only .NET libraries with the .NET Standard 2.0 destination framework.C#
TIP:
The
CSV
file is a part of the sample FactoryTalk Optix Studio
project. You can also download the CSV
file individually from: alarms.csv
TIP:
If you cannot complete this step, save and reopen the project.
TIP:
By default, text boxes retain the typed-in values only if you confirm them by pressing
Enter
on the keyboard.
You can change this behavior by setting the
Value change behavior
property of a text box. Provide Feedback