(optional) Install ControlFLASH or ControlFLASH Plus
Starting from ControlFLASH version 13.00, when the installation completes, FactoryTalk Security is enabled by default. When launched, ControlFLASH logins to the FactoryTalk Network Directory.
TIP:
For details on using ControlFLASH or ControlFLASH Plus, see its documentation.
To install ControlFLASH or ControlFLASH Plus
- Extract the installation package and double-clickSetup.exe.TheRockwell AutomationInstaller appears.
- Follow the instructions to complete the installation process.
Provide Feedback