Main Topic for System Requirements
FactoryTalk® Edge Gateway™
works within the system requirements of all
Rockwell Automation®
software products.Hardware requirements
FactoryTalk Edge Gateway
requires hardware that meets or exceeds these specifications:- 4 GB of memory
- Dual-core processor
Rockwell Automation
recommends at least 32 GB of available drive space for FactoryTalk Edge Gateway
.
TIP:
The hardware footprint affects application sizing. For more information, see
Data flow limits
in Application Notes.Software requirements
FactoryTalk Edge Gateway
requires the following software on the host computer:- Operating systemFactoryTalk Edge Gatewayruns on the followingWindows®operating systems:
- Windows11 Professional or Enterprise edition (64-bit)
- Windows10 Professional or Enterprise edition (64-bit)
- Windows10 IoT Enterprise 2016
- Windows Server2019 Standard
- Windows Server2016 Standard
- Windows Server®2012 R2 Standard
When you install
FactoryTalk Activation Manager
v4.04 the following software will be installed if not already present:FactoryTalk Diagnostics
version 2.90.NET Framework 4.5.2
Wibu CodeMeter runtime version 6.30
Flexera version 11.14
FactoryTalk® Services Platform
6.20.00Provide Feedback