Indicators and LEDs

The IND780 EtherNet/IP Interface which is located inside the IND780 terminal's enclosure is equipped with four status LEDs that are visible on the module itself.
LEDs
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal