Cannot perform reset operation
Cannot perform reset operation because the physical device does not match the configured
device in the project. These parameters must match:
- Vendor
- Product Type and Product Code for a particular Vendor's catalog number
- Major Revision
Provide Feedback