Configure advanced network properties for tap devices
Use
Advanced Network Configuration
to configure advanced network properties.For more information on how to configure the advanced network properties, refer to the EtherNet/IP Embedded Switch Technology Application Guide
(Publication ENET-AP005).
To configure advanced network properties for tap devices
- On the tab for the device, selectNetwork.
- In theNetworkview, selectAdvanced.
- InAdvanced Network Configuration, configure the network properties as needed.
- SelectSetto write the changes to the device.
Provide Feedback