Network view parameters (non-supervisor devices)
The
Network
view for non-supervisor devices includes these parameters.The values only appear when the controller is online and there is no communication error.
Parameter | Description |
|---|---|
Network topology | Displays the current network topology as either:
|
Network status | Displays the current network status as:
|
Refresh | Retrieves the latest information from the device and displays it in the
Network view. |
Provide Feedback