Network view (non-supervisor devices)
Use the
Network
settings to view network information for the port.- View whether the device is operating in a Linear/Star or Device-Level Ring (DLR) network.
- View the current status of the network.
This information is only available when online, and there is no communication error in the
device profile.
Provide Feedback