Connection and Data Format

Change the device definition at any time without deleting the existing device and creating a new device. The profile attempts to display all configuration data for the new settings. Sets to a default value any configuration data that cannot be shown. After applying the new settings, these settings become the base configuration and all previous data format configurations are lost.
Parameter
Description
Input
Generates the input and configuration data types and tags.
If the connection is established, the connection owns the configuration data and shares the input data.
Output
Generates the input, output, and configuration data types and tags.
If the connection is established, the connection owns the configuration and output data and shares the input data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal