Diagnose a problem with an individual channel
Use
Channel0x Diagnostics
to diagnose a problem and view the diagnostics information
for an individual channel. Diagnostics is disabled when:- You are operating offline.
- An Identity mismatch exists.
To diagnose a problem with an individual channel
- On the tab for the device, expandChannels, and then select an individual channel.
- In theCh0xview, selectDiagnostics.
- InChannel0x Diagnostics, view the diagnostics information.
Provide Feedback