Fiber Channel Status
The following procedure shows how to program an MSG instruction to obtain the status
of the dual fiber channels on a 1756-RM3 redundancy module.
- In the program for the redundant controller, create an MSG instruction.
- On the Communication tab of the Message Configuration dialog box, configure a path of THIS to the redundancy module.
- On the Configuration tab of the Message Configuration dialog box, enter the following parameters.ParameterValueMessage TypeCIP GenericService TypeGet Attribute SingleClass56 (hex)Instance1Attribute66 (hex)Destination ElementThe tag that is an array or UDT of two UINTs: first for channel 1 and second for channel 2.
- Download and test the MSG instruction.See the following table for status value definitions.ValueDescription0Status is undetermined because startup is in progress.1The channel is disabled.2The channel is operating normally.3Packets were lost on one channel during the last 60 seconds.4One of these conditions exists:
- Channel 1 is connected to Channel 2.
- The channel has an intermittent loss of communication.
5The connection is down.6The SFP transceiver is not detected, not disabled.7The SFP transceiver is not supported, not disabled. SFP is present.
Provide Feedback