Trust Zone Requirements

For compliance with 62443 4-2 SL1 requirements, a trust zone must be enforced around the redundant chassis and its I/O network. You can use several methods to enforce a trust zone. One method is to allow remote access to the redundant chassis only through a
CIP Security™
-enabled communication module. Physically isolate unsecured devices, such as remote I/O, in a non-converged network.
The following example shows a trust zone configuration for the primary chassis. Apply the same configuration to both primary and secondary chassis.
Trust Zone Configuration Example
Trust zone configuration for primary chassis
Item
Description
A
A
CIP Security™
-enabled 1756-EN4TR communication module is the only method of direct remote access to the redundant chassis. The zone where this module is located must have
CIP™
bridging configured to allow only secure traffic and not allow trusted IP addresses. Star, DLR, and PRP topologies are supported with
CIP Security™
. We recommend including multiple
CIP Security™
-enabled 1756-EN4TR modules per chassis for backup access to the chassis.
B
Physically isolated I/O network. No other direct physical connections are allowed to remote I/O devices except the redundant chassis pair. All remote access to I/O is accomplished through the secured 1756-EN4TR communication module (item A) for updates and maintenance.
A physically isolated, non-converged I/O network provides these protections:
  • All remote access to the chassis is enforced via
    CIP Security™
    zones/conduits while also being verified via x.509 certificates for authentication/authorization.
  • Because the I/O network is connected via Ethernet cables only to the redundant chassis, access to the I/O network is limited:
    • Direct access is possible only via devices in the redundant chassis pair, which can include communication modules other than 1756-EN4TR modules
    • Remote access is possible only via secured 1756-EN4TR modules, which allow authorized access only to the redundant chassis pair
    IMPORTANT:
    Any remote access to the I/O devices for maintenance and updates must be done via the secured 1756-EN4TR module. Other types of network modules, such as
    ControlNet®
    or
    DeviceNet®
    modules, are not supported with Logix SIS or
    ControlLogix®
    5590 redundancy, and must not be used.
  • Isolating the I/O network reduces the attack surface as all remote access to the I/O network passes through the
    CIP Security™
    -enabled communication module.
For defense in depth with non-converged I/O networks, we recommend that you still implement and configure the firewall layers as recommended on the referenced firewall applications.
WARNING:
If you choose to use a converged I/O network, you must use additional measures to prevent unauthorized access to the redundant chassis pair or I/O modules. If the redundant chassis pair contains any Ethernet devices that are visible to the broader network, you must enforce a trust zone to prevent unauthorized access to the Ethernet devices and remote I/O modules.
A firewall is required with converged I/O networks.
While firewall configuration is application-specific, we recommend the following:
  • Use an allow list that provides access only to the following:
    • Specific machines
    • Minimum protocols that are required to communicate to unsecured devices in the redundant chassis pair
  • Protect addresses of devices on both redundant chassis.
  • Place the firewall around the redundant chassis pair and the I/O network that it operates.
    We advise not to place a firewall
    between
    the redundant chassis pair and the I/O network that it operates. A firewall that is configured on the communication path between a controller and its I/O network can introduce risks, such as a compromised safety reaction time or blocked communication between the controller and I/O devices.
For more information about firewall configuration, see the following:
  • PlantPAx Distributed Control System Configuration and Implementation User Manual, publication PROCES-UM100
  • Deploying Industrial Firewalls within a Converged Plantwide Ethernet Architecture Design and Implementation Guide, publication ENET-TD002
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal