Software Installation Requirements and User Permissions
For a secure system, the following software must be installed on the same computer, and
the computer must be separate from the computer that is used for control system
applications:
- FactoryTalk® Policy Manager
- FactoryTalk® Directory
- At least one instance ofFactoryTalk® Linx
You must configure permissions so that all users are authenticated before they can access
the software that is used to access and configure the system, including the Logix
Designer application,
FactoryTalk® Linx
software, and ControlFLASH Plus®
software.Provide Feedback