Configure User Program Control

User program control determines how redundancy modules respond to commands from the controller:
  • To configure the redundancy modules to accept all valid commands via an MSG instruction from a Logix controller, enable user program control.
  • To configure the redundancy modules to reject all commands from a Logix controller, disable user program control.
User program control is disabled by default.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal