Safety Partner Reset

Follow these steps to perform a safety partner reset.
  1. Power down the safety partner.
  2. Use a small tool with a diameter of a paper clip to press and hold the reset button. This button is recessed 5 mm (0.19 in.) behind the panel.
  3. While holding in the reset button, power up the safety partner.
  4. Continue to hold the reset button while the 4-character display cycles through DFLT, 4, 3, 2, 1, Factory Default.
  5. After Factory Default appears, release the reset button
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal