Safety Partner Fault
If the SIL configuration is set to SIL 2 and a safety partner is installed in the slot next the safety primary, these actions occur:
- On the 1756-L9SP safety partner, the MOD status indicator flashes red.
- The controller logs a Type 14, Code 12 minor fault that indicates that the controller is configured for SIL 2, and a safety partner is present.
- The programming application returns an error when an attempt is made to download a SIL 2 application.
Provide Feedback