Safety Faults
Safety systems can experience the following faults.
Nonrecoverable Controller Faults
These faults occur when the internal diagnostics of the controller discovers a fault. If a nonrecoverable controller fault occurs, standard and safety task execution stops and outgoing connections stop. Safety I/O devices respond to the loss of output data by transitioning to the safe state. Recovery requires that you download the application program again.
Nonrecoverable Safety Faults in the Safety Application
If a nonrecoverable safety fault occurs in the safety application, the safety logic and the safety protocol are ended. Safety task watchdog and control partnership faults fall into this category.
When the safety task encounters a nonrecoverable safety fault, a standard major recoverable fault is also logged, and the controller proceeds to execute the controller fault handler, if one exists. If the controller fault handler handles this fault, then the standard tasks continue to run, even though the safety task remains faulted.
ATTENTION:
Overriding a safety fault does not clear the fault. If you override a safety fault, it is your responsibility to prove that operation of your system is still safe.
You must provide proof to your certifying agency that your system can continue to operate safely after an override of a safety fault.
Several nonrecoverable safety faults can be cleared, with or without a safety task signature, to enable the safety task to run. The safety task inoperable fault requires that you download the application again for the safety task to run.
Recoverable Safety Faults in the Safety Application
If a recoverable fault occurs in a safety program, the system can halt the execution of the safety task, depending upon if the Program Fault Handler in the safety program (if one exists) handles the fault.
When a recoverable fault is cleared programmatically, the safety task continues without interruption.
When a recoverable fault in the safety application is not cleared programmatically, a Type 14, Code 2 recoverable safety fault occurs. The safety task execution is stopped, and safety protocol connections are closed and reopened to reinitialize them. Safety outputs are placed in the safe state and the producer of safety-consumed tags commands the consumers to place them in a safe state, as well.
If the recoverable safety fault is not handled, a standard major recoverable fault is also logged, and the controller proceeds to execute the controller fault handler, if one exists. If the controller fault handler handles this fault, then the standard tasks continue to run, even though the safety task remains faulted.
The occurrence of recoverable faults is an indication that the application code is not protecting itself from invalid data values or conditions. Consider modifying the application to reduce the risk of these faults, rather than handling them at runtime.
View Faults
The Recent Faults dialog box on the Major Faults tab of the Controller Properties dialog box contains two subtabs, one for standard faults and one for safety faults.
The status display on the controller also shows fault codes with a brief status message. For more information about status indicators, see the following:
Fault Codes
Safety controllers show fault codes on the Major Faults tab of the Controller Properties dialog box and in the PROGRAM object, MAJORFAULTRECORD or MINORFAULTRECORD attribute.
IMPORTANT:
This manual links to Logix 5000 Controller and I/O Fault Codes and Syslog Messages, 1756-RD001; the file automatically downloads when you click the link.
Provide Feedback