SMTP Server

The SMTP server is only available via the enterprise port. Therefore, emails can only be sent on the enterprise port.
For more information on how to send emails via an Ethernet port, see the EtherNet/IP Network Configuration User Manual, publication ENET-UM001.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal