Change the EtherNet/IP Mode in the Logix Designer Application
This example shows the
EtherNet/IP™
mode change from Dual-IP mode to Linear/DLR mode. The same tasks apply to change from Linear/DLR mode to Dual-IP mode
IMPORTANT:
With
ControlLogix®
5590 controllers, the Ethernet ports on the controller itself are labeled 1 and 2. In programming and communication software, the ports are described as A1 and A2.Make sure that you are aware of the effects of changing the
EtherNet/IP™
mode. See Change the EtherNet/IP Mode.- Confirm that the project is offline.
- On the General tab of the Controller Properties dialog box, click Change IP Mode.

- From the New mode dropdown, choose the new mode and click OK.

- Click OK on the Controller Properties dialog box.
- Save the project.
- Download the updated project to the controller.
- When the following warning appears, read it carefully.
- Click Yes to continue.

Provide Feedback