Requirements for Resource Availability
Security Component | Required to Meet IEC‑62443-4-2 SL 1 | Details |
|---|---|---|
FactoryTalk® AssetCentre software | Yes | Configure and use the following:
For more information, see Configure System Security Features User Manual, SECURE-UM001. |
UPS | Yes | Provide your own UPS with a separate battery unit and redundant power supplies. Size the UPS so that is correctly supports the system and provides enough power to shut down servers and workstations properly. |
Provide Feedback