Disable Controller Webpages via Controller Properties
You can use one of the following methods to disable the controller webpages:
- If the controller web pages are enabled, disable them by clearing the Enable Controller Web Pages check box on the Security tab for the controller properties.
IMPORTANT:The status of the Enable Controller Web Pages checkbox is saved to and restored from the memory card when using the save/restore feature. - ForCIP Security™applications, you can also useFactoryTalk® Policy Managerto disable the webpages (this overrides the Controller Properties checkbox).
Provide Feedback