Jump to the Fault Routine
In the main routine of the program, enter the following rung, where:
- Fault_Routine_1 is the name of the fault routine for the program.
- 999 is the value for the fault code.

When Tag_1.0 = 1, execution jumps to name_of_fault_routine, a major fault occurs and the controller enters the faulted mode. Outputs go to the faulted state. The Controller Properties dialog box, Major Faults tab, displays the code 999.

Provide Feedback