Use the Network Browser to Upload from the Controller
When you upload a project from the controller, it copies the project from the controller to the
Studio 5000 Logix Designer®
application.You can use the features of the Network Browser dialog box to upload from your controller after you have set the communication path.
Complete these steps to upload from the controller.
- After choosing the communication path, click Upload.

- On the Connected to Upload dialog box, verify the project to upload and click Upload.

Provide Feedback