Use the Logix Designer Application to Change the Operation Mode
When you are online with the controller, and the switch position is set to REM, then you can use the Logix Designer application to change the operation mode.
The Controller Status menu lets you specify these operation modes:
- Remote Program
- Remote Run
- Remote Test
From the Controller Status pulldown menu, choose the operation mode.
Operation Modes in Logix Designer

Provide Feedback